AXIS#.PL.CMD.FBUSOFFSET

Description

This parameter displays the position loop feed forward value injected by the fieldbus. The loops are updated every cyclic fieldbus cycle. The fieldbus controller manages jumps in position command due to this feed forward when starting, stopping, switching opmodes, and all other transitions.

Versions

Action Version Notes
Implemented 02-05-05-000

 

Revised 02-08-02-000 Keyword renamed from AXIS#.FBUS.PL.FF

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units.

Range

Depends on units. See Position Range.

Default Value

0

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.PL.CMD.FBUSOFFSET

60b0h

00h

Signed32

Position

-

Read/Write

Yes

AXIS2.PL.CMD.FBUSOFFSET

68b0h

00h

Signed32

Position

-

Read/Write

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.CMD.FBUSOFFSET

5922

1722

Signed32

Read/Write

Position

AXIS2.PL.CMD.FBUSOFFSET

71458

1172

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.CMD.FBUSOFFSET

5922

Signed32

Read/Write

Position